2.2.2021
Simplify Project Design with Atkore’s Revit® Toolbar
Customizable toolbar puts product BIM models at your fingertips
Harvey, Illinois (February 2, 2021) – Atkore International, a leading provider of electrical, safety and infrastructure solutions, has launched its new Revit® Toolbar. The Atkore Revit Toolbar allows users to import BIM (building information modeling) models into their designs without having to leave the Revit software to search multiple websites for the products they need. Using Atkore’s Revit Toolbar simplifies project designs with easy access to Atkore product models.
Some of the toolbars main functionalities include:
Access to Atkore product families
Close to 650 Atkore product families are available for import within the Revit Toolbar. Select the product and product type as well as the product category and category type and the toolbar will provide the corresponding BIM model.
Library Manager
The toolbar is completely customizable from one project to the next. The user has the option to pick and choose which products and product categories they would like to import in the toolbar for each project.
Contact Support
The Revit Toolbar provides a direct line of communication via the phone number and email of an Atkore technical sales representative based on the users location. Users can ask technical and application questions in order to get more information on the products in the toolbar.
Immediate Feedback
Allows users to provide feedback to the Atkore development team regarding additional functionalities and products as well as functionality errors.
Users only need to download and install the toolbar in the Revit software once. After the initial launch, it will automatically run in the background and can be accessed during any project.
Get additional information and download the new Revit Toolbar.
About Atkore International
Atkore is forging a future where our employees, customers, suppliers, shareholders and communities are building better together – a future focused on serving the customer and powering and protecting the world.
With approximately 3,700 employees and 66 manufacturing and distribution facilities worldwide, Atkore is a leading provider of electrical, safety and infrastructure solutions. To learn more, please visit www.atkore.com.